Operator NativeTrgPortInExt

Operator Library: Hardware Platform

The operator NativeTrgportInExt provides an interface to the microEnable's digital inputs. Accessible by the operator are all eight input trigger pins.

Available for Hardware Platforms
microEnable IV VD1-CL/-PoCL

I/O Properties

Property Value
Operator Type M
Output Links TrgI1, signal output
TrgI1..TrgI8, signal output

Supported Link Format

Link Parameter Output Link TrgI1 Output Link TrgI1..TrgI8
Bit Width 1 TrgI[1]]
Arithmetic unsigned TrgI[1]
Parallelism 1 TrgI[1]
Kernel Columns 1 TrgI[1]
Kernel Rows 1 TrgI[1]
Img Protocol VALT_SIGNAL TrgI[1]
Color Format VAF_GRAY TrgI[1]
Color Flavor FL_NONE TrgI[1]
Max. Img Width any TrgI[1]
Max. Img Height any TrgI[1]

Parameters

None